LPC54608 with mcuxpresso IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54608 with mcuxpresso IDE

ソリューションへジャンプ
1,828件の閲覧回数
prathap_ponnuch
Contributor I

Hi,

I am new to this LPC54608.

I am using MCUXPRESSO IDE. For that I download LPC54608 SDK and imported into IDE.

In this SDK all the peripherals are made up of separate projects. But I want to start new project and include each peripherals into it and run. How to do it?Is there any documents or tools available?

Thanks in advance.

regards,

prathap

ラベル(1)
0 件の賞賛
返信
1 解決策
1,761件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi ,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
In the MCUXpresso, it provides a GUI plug-in tool to create a new project quickly, and you can learn more information about it via going through chapter 5. Creating New Projects using installed SDK Part Support.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,762件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi ,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
In the MCUXpresso, it provides a GUI plug-in tool to create a new project quickly, and you can learn more information about it via going through chapter 5. Creating New Projects using installed SDK Part Support.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信