LPC54608 to manage acceleration and deceleration with a stepper motor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC54608 to manage acceleration and deceleration with a stepper motor

629 Views
AntoineB
Contributor I

Hello,

I need to generate a signal from a CTIMER to feed a stepper motor drive to control the speed of the motor and to being able to count the number of pulse I generated and stop the signal when an number of pulses have been reach.

I succeed to do it at constant speed (when I don't need to change the frequency of my signal) by doing like this :

// To start my timer

CTIMER_StopTimer(CTIMER1);

CTIMER_Reset(CTIMER1);
CTIMER_SetupPwm(CTIMER1, CTIMER_MAT_OUT, 50, freq, CTIMER1_TICK_FREQ, false);
CTIMER_StartTimer(CTIMER1);

// To count the number of pulses before to stop motor

void CTIMER1_Callback_interrupt(uint32_t flags)
{

countIncMotor++;
if( countIncMotor >= M1_stepsNumberToRun) // arret moteur nombre de pas atteint
{
Moteurs.b.bOnOffM1 = false;
CTIMER_StopTimer(CTIMER1);
GPIO_PinWrite(GPIO, MOTOR1_INIT_ENABLE_PORT, MOTOR1_INIT_ENABLE_PIN, 1);
printf("Pulse motor stop, pulse idx =%d\n",countIncMotor );
}

}

When I don't change the frequency signal during motor is on, no problem the number of speed counted by the CTIMER1_Callback_interrupt correspond to the number of pulses observed on the oscilloscope and the motor stop at expected position. 

 

But when I had some acceleration and deceleration during motor movement the motor finished always with a position with more steps than expected almost like if the callback missed some pulses during PMW reinitialization. Do you see any work around to avoid this problem?

How I do to change the frequency :

// loop task 
while(1)
{

DelayMS(TIME_BETWEEN_FREQ_CHANGE_IN_MS);
if(Moteurs.b.bOnOffM1)
{
if( nbLoopOccured == 0 ) M1_currentFreq = M1_miniFreq;
if( nbLoopOccured < (M1_maxFreq - M1_miniFreq)/M1_freqDiff)  // acceleration
{
CTIMER_StopTimer(CTIMER1);
CTIMER_Reset(CTIMER1);
M1_currentFreq = M1_currentFreq + M1_freqDiff;
CTIMER_SetupPwm(CTIMER1, CTIMER_MAT_OUT, 50, M1_currentFreq, CTIMER1_TICK_FREQ, false);
CTIMER_StartTimer(CTIMER1);
printf("acceleration %d < %d freq:%d\n", (nbLoopOccured), (M1_maxFreq - M1_miniFreq)/M1_freqDiff , M1_currentFreq);
}
else  // deceleration
{
if( M1_currentFreq> M1_miniFreq)
{
CTIMER_StopTimer(CTIMER1);
CTIMER_Reset(CTIMER1);
M1_currentFreq = M1_currentFreq - M1_freqDiff;
CTIMER_SetupPwm(CTIMER1, CTIMER_MAT_OUT, 50, M1_currentFreq, CTIMER1_TICK_FREQ, false);
CTIMER_StartTimer(CTIMER1);
printf("deceleration %d < %d freq:%d\n", (nbLoopOccured), (M1_maxFreq - M1_miniFreq)/M1_freqDiff , M1_currentFreq);
}
}

 

 

 

 

Labels (1)
0 Kudos
Reply
1 Reply

590 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @AntoineB 

 

If using LPC54608 control motor, recommend you use SCTIMER. How about using it, check whether can resolve your issue.

 

BR

Alice

0 Kudos
Reply