LPC54608 eva board ISP,SDRAM pin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54608 eva board ISP,SDRAM pin

1,319件の閲覧回数
実奥山
Contributor II

CPU packege is 180-pin, TFBGA  in OM13092 board

C8 pin is connected to SDRAM and ISP switch.

There is a 2.2K resistor(R108) between the ISP switch and the CPU.

Why are you using a 2.2K resistor?

Shouldn't it be a 0 ohm resistor?

ラベル(1)
0 件の賞賛
返信
1 返信

1,214件の閲覧回数
carstengroen
Senior Contributor II

My guess would be to protect the CPU if the ISP switch is pressed while the pin is used for accessing SDRAM. The 2.2K resistor will limit the current if switch is pressed during SDRAM access, at the same time its value is low enough to pull the pin low during boot (and activate ISP)