LPC54607 Run functions into sdram

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC54607 Run functions into sdram

1,792 次查看
omeraygor
Contributor I

Hi,

My problem is about MCU flash size. Flash size is not enough for me. So want to some of fonctions put into sdram.

in the document, https://www.nxp.com/docs/en/application-note/AN12423.pdf

There is memory allocation section , i saw something like that ;

#define m_sdram_start 0xA0000000
#define m_sdram_size 0x80000
LR_m_sdram_text m_sdram_start m_sdram_size {
*(SDRAM_Data)
*(SDRAM_Function)
core_list_join.o
core_matrix.o
core_state.o
core_util.o
} 

This is part of linker file. 

what does it mean? So core_list_join.o located sdram and others into flash?

 

i added this into linker file. My fille is;

#!armclang --target=arm-arm-none-eabi -mcpu=cortex-m4 -E -x c
/*
** ###################################################################
**     Processors:          LPC54607J256BD208
**                          LPC54607J256ET180
**
**     Compiler:            Keil ARM C/C++ Compiler
**     Reference manual:    LPC546xx User manual Rev.1.9  5 June 2017
**     Version:             rev. 1.2, 2017-06-08
**     Build:               b190923
**
**     Abstract:
**         Linker file for the Keil ARM C/C++ Compiler
**
**     Copyright 2016 Freescale Semiconductor, Inc.
**     Copyright 2016-2019 NXP
**     All rights reserved.
**
**     SPDX-License-Identifier: BSD-3-Clause
**
**     http:                 www.nxp.com
**     mail:                 support@nxp.com
**
** ###################################################################
*/


; normal flashdan çalisma.
#define m_interrupts_start             0x00000000
#define m_interrupts_size              0x00000400

#define m_text_start                   0x00000400
#define m_text_size                    0x0003FC00

#define m_data_start                   0x20000000
#define m_data_size                    0x00018000

#define m_usb_sram_start               0x40100000
#define m_usb_sram_size                0x00002000

#define m_sdram_start 				   0xA0000000
#define m_sdram_size 				   0x80000
LR_m_sdram_text m_sdram_start m_sdram_size {
*(SDRAM_Data)
*(SDRAM_Function)
core_list_join.o
core_matrix.o
core_state.o
core_util.o
} 

/* USB BDT size */
#define usb_bdt_size                   0x0
/* Sizes */
#if (defined(__stack_size__))
  #define Stack_Size                   __stack_size__
#else
  #define Stack_Size                   0x0400
#endif

#if (defined(__heap_size__))
  #define Heap_Size                    __heap_size__
#else
  #define Heap_Size                    0x0400
#endif

LR_m_text m_interrupts_start m_text_start+m_text_size-m_interrupts_start { ; load region size_region
  VECTOR_ROM m_interrupts_start m_interrupts_size { ; load address = execution address
    * (.isr_vector,+FIRST)
  }
  ER_m_text m_text_start FIXED m_text_size { ; load address = execution address
    * (InRoot$$Sections)
    .ANY (+RO)
  }

  RW_m_data m_data_start m_data_size-Stack_Size-Heap_Size { ; RW data
    .ANY (+RW +ZI)
  }
  ARM_LIB_HEAP +0 EMPTY Heap_Size {    ; Heap region growing up
  }
  ARM_LIB_STACK m_data_start+m_data_size EMPTY -Stack_Size { ; Stack region growing down
  }
}

LR_m_usb_bdt m_usb_sram_start usb_bdt_size {
  ER_m_usb_bdt m_usb_sram_start UNINIT usb_bdt_size {
    * (*m_usb_bdt)
  }
}

LR_m_usb_ram (m_usb_sram_start + usb_bdt_size) (m_usb_sram_size - usb_bdt_size) {
  ER_m_usb_ram (m_usb_sram_start + usb_bdt_size) UNINIT (m_usb_sram_size - usb_bdt_size) {
    * (*m_usb_global)
  }
}

 

But i got errors while compiling.

This is Error:

debug\AIRHMI_NXP_7_INCH_1v0.axf: Error: L6630E: Invalid token start expected number or ( but found S at position 3 on line 12
debug\AIRHMI_NXP_7_INCH_1v0.axf: Error: L6629E: Unmatched parentheses expecting ) but found S at position 3 on line 12
debug\AIRHMI_NXP_7_INCH_1v0.axf: Error: L6226E: Missing base address for region *.
C:\Users\omera\AppData\Local\Temp\p5248-3(12): error: L6292E: Ignoring unknown attribute 'SDRAM_Data' specified for region *.
C:\Users\omera\AppData\Local\Temp\p5248-3(12): error: L6228E: Expected '{', found ')...'.
C:\Users\omera\AppData\Local\Temp\p5248-3(12): error: L6228E: Expected '}', found 'EOF'.
Not enough information to list image symbols.
Not enough information to list load addresses in the image map.
Finished: 2 information, 0 warning and 6 error messages.
"debug\AIRHMI_NXP_7_INCH_1v0.axf" - 6 Error(s), 0 Warning(s).
Target not created.
Build Time Elapsed:  00:00:01

 

 

 

 

标签 (1)
0 项奖励
回复
4 回复数

1,771 次查看
omeraygor
Contributor I

Hi again,

i wrote a bootloader, it can be coppy code from external flash to sdram. then execute code from there. But executing from sdram is very slower.

so i want to that bootloader copy some of code sdram and main code is in the flash another location. 

Can CPU do that? 

a part of code in the sdram execute and main code inside flash memory?

0 项奖励
回复

1,764 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Regarding your question that you copy code from SDRAM to another location of flash, I suppose the so-called flash is on-chip flash, we provide IAP function which can program on-chip flash.

For detailed inf, pls refer to Chapter 5: LPC546xx ISP and IAP in UM10912.pdf, the SDK also provides the IAP example code.

Hope it can help you

BR

XiangJun Rong

0 项奖励
回复

1,781 次查看
frank_m
Senior Contributor III

> My problem is about MCU flash size. Flash size is not enough for me. So want to some of fonctions put into sdram.

For a MCU like the LPC546xx, RAM is hardly a solution for overflowing Flash.

Any code to be executed from RAM is copied at runtime from Flash first. You could use external Flash, like QSPI Flash. Or a MCU variant with larger Flash instead.

But for a MCU with limited RAM like Cortex M devices, code execution from RAM most often used for IAP code. Most of this MCUs have only one Flash bank, which cannot execute code while erasing/writing any sector in that bank is ongoing.

0 项奖励
回复

1,783 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Omer,

As you know that the SRRAM is volatile memory, after power off, the data/code in SDRAM will disappear.

You have to save code/data in on-chip flash or external flash, if you extend external flash for example spi flash or parallel flash accessed by EMC, it is okay. For example, you can compile a function as data array and save them in external spi flash, after power-on, copy them to on-chip SRAM or SDRAM, then execute.

You can change another LPC processor with large on-chip flash.

 

Hope it can help you

BR

XiangJun Rong

0 项奖励
回复