Hi,
We selected LPC54606J256ET180E to develop portable printer, which connects to PC by USB1 in HS mode.
Before, our printer works well in windows7 or windows10, but when connects to windows11, USB1 interface will handshake to windows11 for about 10s, then change to FS mode.
Meanwhile, we test the printer with STM32F723, it is quick to connect in FS mode.
We have checked the LPC5460x Reference Manual, but can't find any option to fix this problem.
Hope you can provide us some tips to fix.
Thanks very much.
----Test log:
链接:https://pan.baidu.com/s/1Y8wAkuImzBDNYXKWV1DFHw
提取码:jjrj
 
					
				
		
 ZhangJennie
		
			ZhangJennie
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi jimmyli
Did you test USB1 with one of MCUXpresso SDK USB demo code?
Jun Zhang
Hi Jennie,
Yes, we have verified with the offical demo, and the phenomenon is the same.
Demo: LPCXpresso54628
SDK: SDK_2_10_0_LPCXpresso54628\boards\lpcxpresso54628\usb_examples\usb_device_printer_virtual_plain_text\bm
Thanks.
 
					
				
		
 ZhangJennie
		
			ZhangJennie
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Thanks.
I need to check it more internally. Please send me this information:
1. your project application name( scenarios of your application)
2. I don't have a win11 to test. please provide me the problem related screenshot.
Thanks for your cooperation.
Jun Zhang
Hi Jun,
Project name: thermal printer connecting to PC by usb port.
Screen shot: below is the log that customer grabs from the test screen.
link:https://pan.baidu.com/s/1Y8wAkuImzBDNYXKWV1DFHw
password:jjrj
Thanks.
 
					
				
		
 ZhangJennie
		
			ZhangJennie
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		What I downloaded from this file is USB ANALYZER.zip. Not log file and screenshot.
Could you please confirm if this is correct one?