LPC546 MCAN not sending data continuously.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC546 MCAN not sending data continuously.

2,139件の閲覧回数
emb02
Contributor V

I am trying to interface MCAN and want to send data continuously but when I disconnect CAN H or CAN L line it will sets error and giving kStatus_MCAN_TxBusy status. it is not giving idle status when i connect line again. please help me to continuous communication between CAN. I am initiating can using config tools.

ラベル(2)
タグ(3)
0 件の賞賛
返信
3 返答(返信)

2,120件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

What do you mean "when I disconnect CAN H or CAN L line"? do you means that you disconnect both the CAN H or CAN L line between transmitter and receiver nodes?

BR

XiangJun Rong

0 件の賞賛
返信

2,115件の閲覧回数
emb02
Contributor V
yes I am disconnecting CAN H, CAN L .
0 件の賞賛
返信

2,111件の閲覧回数
frank_m
Senior Contributor III

Educate yourself about the meaning of transmit / receive errors, error passive state, and bus-off state, which are intrinsic part of the CAN specification.

0 件の賞賛
返信