LPC5411x - Boot loader with In-System Programming (ISP) over USB issue?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC5411x - Boot loader with In-System Programming (ISP) over USB issue?

跳至解决方案
3,554 次查看
robbc
Contributor II

I just got the LPC5411x dev board (OM13089) and was trying to program the micro using the boot mode ISP feature over USB.  I followed the procedures on UM10973 - section 9.2 and it worked successfully when Vdd is 3.3V.  

 

The board has a selectable Vdd option of 1.8V or 3.3V using J9.  If I switch to Vdd = 1.8V and try and the same boot procedure using USB, it does not work.  If I replace the jumper and switch back to Vdd = 3.3V the device is recognized and I can see it on my computer.  

I have 2 boards and the both behave the same.

 

Questions:

 1) Has anyone tried this or seen the same behavior? Is it specific to the dev board or to the micro?

2)Do you need 3.3V to enter ISP boot mode over using USB and flash? Is this documented somewhere?

3) I would like to power everything with 1.8V –what are my options if I want to still flash over USB?

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
3,305 次查看
robbc
Contributor II
0 项奖励
回复
4 回复数
3,305 次查看
ckphua
NXP Employee
NXP Employee

To have USB running on the LPC5411x, the VDD should be >3.0V. This is stated in the Datasheet. Switching to 1.8V will make the USB function not functioning.

If you want to run LPC5411x with USB, you will need to boost the 1.8V to 3.0V on your board.

0 项奖励
回复
3,305 次查看
robbc
Contributor II

Thanks for the quick reply.  Can you please be more specific as to where in the datasheet this is specified.

0 项奖励
回复
3,305 次查看
ckphua
NXP Employee
NXP Employee

Please refer to 11.14 USB Interface characteristic on  Datasheet... Top of Table 34

0 项奖励
回复
3,306 次查看
robbc
Contributor II

Thanks.

0 项奖励
回复