LPC54018 Flash ended with an error.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC54018 Flash ended with an error.

1,741 Views
Sukumar_M
Contributor I

Hi, 

 I have some problem on LPC54018 OM40003 EVK . First board same problem occur so new board changed but now this board also same problem occurs.so please anyone say how to solve this problem. I'm new from MCUxpresso so please anyone give me solution.

Writing 11772 bytes to address 0x10000000 in Flash
1 of 1 ( 0) Writing sectors 0-0 at 0x10000000 with 11772 bytes
( 0) at 10000000: 0 bytes - 0/11772
Program Page (0x10000000, 0x22B8, 0x4000) status 0x1 - driver reported driver error - EXTSPI driver rc -20 (0xFFFFFFEC)
Sectors written: 1, unchanged: 0, total: 1
Closing flash driver LPC540xx_SPIFI_SFDP.cfx
(100) Writing Flash ended with an error.
File 'lpcxpresso54018_gpio_led_output.axf' load failure: Ef(49): Flash driver operation gave error.
(100) Target Connection Failed
Unable to perform operation!
Command failed with exit code 1

Labels (1)
0 Kudos
Reply
2 Replies

1,685 Views
Sukumar_M
Contributor I

Thanks for Support to me.

0 Kudos
Reply

1,720 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Sukumar_M,

I believe your problem is basically the same error as the one described in this post:

https://community.nxp.com/t5/MCUXpresso-IDE/I-can-not-program-file-into-flash-by-MCUXpressIDE/m-p/92...

Please follow the steps described by my colleague and let me know if it works.

 

BR,

Edwin.

0 Kudos
Reply