LPC54005 SPIFI boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54005 SPIFI boot

1,747件の閲覧回数
michaelbotham
Contributor I

On an LPC54005, does the SPIFI boot ROM assume there is an external xtal?

Reason for asking is that my board will not boot, and the lack of xtal is the only difference I can see between my board and the development board.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,617件の閲覧回数
michaelbotham
Contributor I

Found the problem, SPIFI device not programmed correctly.However I did find that the MCUXpresso SPIFI driver will fail to initialize without a crystal, so you do need a crystal to debug.

0 件の賞賛
返信

1,617件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Michael,

Thanks for sharing this information.

Best Regards,

Alexis andalon

0 件の賞賛
返信

1,617件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Michael,

If you look in the reference manual in the section 3.4.3 SPIFI boot mode it mention the steps need it, what you could check is the image header and see if its valid or not.

Let me know if this is helpful to you.

Best Regards,

Alexis Andalon

0 件の賞賛
返信