LPC43XX source not list in MCUXpresso SDK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC43XX source not list in MCUXpresso SDK

2,216件の閲覧回数
robberpen
Contributor III

Hi

I download  MCUXpresso newest SDK

But I can not see LPC43XX from IDE "Home->Download and Install SDKs"

It can only list LPC5XX series, cannot see any PLC4XX series. any hint?

Regards

Peter

 

image.png

0 件の賞賛
返信
5 返答(返信)

2,203件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @robberpen 

HangZhang_0-1709878606049.png

According to the picture, you should select Import projects from file system->Browse->LPCOpen,

and you will see LPC43XX series.

I hope I can help you.

Best regards,
Hang

 

 

0 件の賞賛
返信

2,197件の閲覧回数
robberpen
Contributor III
It seems you means LPC43XX source code not included in SDK. by default.
That is , I need download LPC34xx source code from offical web-site, then import manually, right?
Where could I download Project source code? I cannot found from NXP web-site?
0 件の賞賛
返信

2,147件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @robberpen 

There is no SDK for LPC43XX on the official website, but in MCUXpesso IDE file system. 

So you should open the MCUXpesso IDE and follow the picture in the previous comment.

Select Import projects from file system->Browse->LPCOpen

 

Best regards,

Hang

0 件の賞賛
返信

2,119件の閲覧回数
robberpen
Contributor III
I installed MCUXpressoIDE_11.9.0_2144 for chip LPC43s70fet100

Due to I have no LPC43s70fet100 board so far. that is what the wizard could not detect my device board perporly

1. Did you means below path is what I need to import?

>D:\nxp\MCUXpressoIDE_11.9.0_2144\ide\plugins\com.nxp.mcuxpresso.tools.wizards_11.9.0.202307121226\Examples\LPCOpen\lpcopen_2_12_lpcxpresso_nxp_lpclink2_4370_g

2. Not sure "lpcopen_2_12_lpcxpresso_nxp_lpclink2_4370_g" is what I need or not.

This is my first in NXP MCU LPC series. And it is helpful if you can share me what is the exactly project pathname
0 件の賞賛
返信

1,546件の閲覧回数
MLH
Contributor I
0 件の賞賛
返信