LPC43XX source not list in MCUXpresso SDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC43XX source not list in MCUXpresso SDK

2,224 Views
robberpen
Contributor III

Hi

I download  MCUXpresso newest SDK

But I can not see LPC43XX from IDE "Home->Download and Install SDKs"

It can only list LPC5XX series, cannot see any PLC4XX series. any hint?

Regards

Peter

 

image.png

0 Kudos
Reply
5 Replies

2,211 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @robberpen 

HangZhang_0-1709878606049.png

According to the picture, you should select Import projects from file system->Browse->LPCOpen,

and you will see LPC43XX series.

I hope I can help you.

Best regards,
Hang

 

 

0 Kudos
Reply

2,205 Views
robberpen
Contributor III
It seems you means LPC43XX source code not included in SDK. by default.
That is , I need download LPC34xx source code from offical web-site, then import manually, right?
Where could I download Project source code? I cannot found from NXP web-site?
0 Kudos
Reply

2,155 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @robberpen 

There is no SDK for LPC43XX on the official website, but in MCUXpesso IDE file system. 

So you should open the MCUXpesso IDE and follow the picture in the previous comment.

Select Import projects from file system->Browse->LPCOpen

 

Best regards,

Hang

0 Kudos
Reply

2,127 Views
robberpen
Contributor III
I installed MCUXpressoIDE_11.9.0_2144 for chip LPC43s70fet100

Due to I have no LPC43s70fet100 board so far. that is what the wizard could not detect my device board perporly

1. Did you means below path is what I need to import?

>D:\nxp\MCUXpressoIDE_11.9.0_2144\ide\plugins\com.nxp.mcuxpresso.tools.wizards_11.9.0.202307121226\Examples\LPCOpen\lpcopen_2_12_lpcxpresso_nxp_lpclink2_4370_g

2. Not sure "lpcopen_2_12_lpcxpresso_nxp_lpclink2_4370_g" is what I need or not.

This is my first in NXP MCU LPC series. And it is helpful if you can share me what is the exactly project pathname
0 Kudos
Reply

1,554 Views
MLH
Contributor I
0 Kudos
Reply