LPC43XX: General Purpose DMA doc?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC43XX: General Purpose DMA doc?

5,036件の閲覧回数
a_bet
Contributor IV

Hi to you all,
as I already pointed out (LPC43XX: Timer triggered DMA transfer? ) I'm having a lot of troubles using the GPDMA on LPC4370.
Searching the web I found this useful doc: https://www.mikrocontroller.net/attachment/28181/gpdma.pdf (attached below, also)
Unfortunately as you can read is "a draft full of errors", is there an updated version of this doc?
Or another resource I can use, I'm a bit stuck at the moment.

Thank you in advance.

Andrea

ラベル(3)
タグ(4)
4 返答(返信)

4,399件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Andrea Bettati,

Thank you for your interest in NXP Semiconductor products and 

for the opportunity to serve you.
I've amended the LPCOpen demo to meet your goal which setup the match event to trigger the DMA transferring.
And you can learn the detailed reply in the https://community.nxp.com/thread/446219
Have a great day!

Best regards,

Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

4,399件の閲覧回数
a_bet
Contributor IV

Hi jeremyzhou‌ thanks for the reply. I think that this peripheral is complex: other company have Application Notes about the functioning of their DMAs, are there some resources of this kind from NXP regarding the GPDMA in LPC43XX?

0 件の賞賛
返信

4,399件の閲覧回数
leecoakley
Contributor III

Old question, but for the benefit of those searching - which was me last week! - here is a link to the ARM documentation for the GPDMA block (PL080).  It goes into considerable detail and I was able to implement a nice driver based on this and the NXP docs.

4,399件の閲覧回数
a_bet
Contributor IV

Oh man if I only had found this while working on my thesis...

0 件の賞賛
返信