LPC43S67 floating point

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC43S67 floating point

1,656 次查看
john_schooling
Contributor I

Do the LPC4367 and LPC43S67 have M4F (with FPU) or is it just an M4?

标签 (1)
0 项奖励
回复
2 回复数

1,529 次查看
leecoakley
Contributor III

All the optional features are present. It has the FPU, ITM, ETM, MPU, Systick, 6c/2d breakpoints, and I think eight levels of NVIC priority.

Also worth noting that the secondary M0 cores don't have the fast multipliers, but the 32-cycle ones.

1,529 次查看
soledad
NXP Employee
NXP Employee

Hi,

The LPC43S67 and LPC4367 contain the ARM Cortex-M4 which is a hardware Floating Point Unit (FPU).


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复