LPC43S67 floating point

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC43S67 floating point

1,744件の閲覧回数
john_schooling
Contributor I

Do the LPC4367 and LPC43S67 have M4F (with FPU) or is it just an M4?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,617件の閲覧回数
leecoakley
Contributor III

All the optional features are present. It has the FPU, ITM, ETM, MPU, Systick, 6c/2d breakpoints, and I think eight levels of NVIC priority.

Also worth noting that the secondary M0 cores don't have the fast multipliers, but the 32-cycle ones.

1,617件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

The LPC43S67 and LPC4367 contain the ARM Cortex-M4 which is a hardware Floating Point Unit (FPU).


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信