LPC4370 labtool firmware

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC4370 labtool firmware

1,268 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mshrestha789 on Wed Jul 23 07:58:48 MST 2014
Hello friends,

I've been using lpc-link 2 for my project. I've labtool board from embedded artist as well. I want to use that board for my application.

The problem I am facing right now is when ever I connect lpc-link 2 with the labtool, although I've fully erased microcontroller, the led in the labtool board starts blinking, and when I check through oscilloscope I can also see some data in MOSI pin of the board.

Please help me regarding this problem.

标签 (1)
0 项奖励
回复
1 回复

1,234 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by andersrosvall on Wed Jul 23 13:53:45 MST 2014
Hi,
The signal/LED activity you see comes from the on-board demo signal MCU (an LPC812). The demo signals are generated from this MCU and not from the LPC-Link2 MCU (the LPC4370).
Kind Regards,
Anders from EA
0 项奖励
回复