LPC4370 SPI to SD card (Link 2)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4370 SPI to SD card (Link 2)

971件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by csuteja on Thu Mar 10 05:55:59 MST 2016
Hi,

I have been using SSP1 as SPI to write to a SD card. I used FATFS library online.
However, it stops working when I set the SSP clock rate to 6MHz. The sample code in LPC1769 shows that the default clock rate is 20MHz.
Has anyone encounter this problem before?
Please advise. Thanks
ラベル(1)
0 件の賞賛
返信
1 返信

906件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信