LPC4370 SPI to SD card (Link 2)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4370 SPI to SD card (Link 2)

970 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by csuteja on Thu Mar 10 05:55:59 MST 2016
Hi,

I have been using SSP1 as SPI to write to a SD card. I used FATFS library online.
However, it stops working when I set the SSP clock rate to 6MHz. The sample code in LPC1769 shows that the default clock rate is 20MHz.
Has anyone encounter this problem before?
Please advise. Thanks
Labels (1)
0 Kudos
Reply
1 Reply

905 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply