LPC4330 Custom Bootloader Request

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4330 Custom Bootloader Request

1,139 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by fweller on Thu Mar 10 09:49:01 MST 2016
Our goal is to develop a custom boot loader that will upgrade an internal SPIFI (QSPI) application image with a file loaded from a removable SD Card.

We are requesting example code for this bootloader.
We could also use a good description of how this should be implemented, especially how to set up a LPCXpresso linker environment to build the main application that the bootloader would jump to when it is ready to execute from the SPIFI (SPI) application image.


Labels (1)
0 Kudos
Reply
1 Reply

1,078 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply