LPC4370 HSADC with DMA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4370 HSADC with DMA

2,062件の閲覧回数
mtenw
Contributor I

Hi all,

I have been looking for example codes for HSADC using DMA on LPC-Link2 board. All sources I could find seems to point to the Labtool code. There is no example code using the current lpcopen 2.12 library.

Question:

Is there an example code using lpcopen 2.12? If yes, can you kindly point out the source? If not, any reasons that it does not exist? (For example, maybe lpcopen 2.12 is not able to support the feature?)

Thanks in advance!

ラベル(1)
0 件の賞賛
返信
1 返信

1,482件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi mtenw,

The resources we have on HSADC are LPCOpen examples and the Labtool solution for now, but I think the following thread might be helpful for you:

How to achieve 80MHz using DMA from LPC4370's HSADC?

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 件の賞賛
返信