LPC436x CAN Errata C_CAN.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC436x CAN Errata C_CAN.1

724 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by strontium on Tue Mar 29 23:42:06 MST 2016
The Errata for ALL other 43xx devices contains Errata C_CAN.1, writing to CAN registers corrupts other peripherals on the same BUS
But, i note this Errata is not present in the LPC436x Errata sheet.

In application, I would love to use CAN and the I2C on the same bus, at the same time, and if this Errata is corrected in this device it would be enough to convince me to select it over the LPC4330.

Can anyone CONFIRM that this errata is truly corrected in this device, and not just overlooked in the Errata sheet?
Labels (1)
0 Kudos
Reply
2 Replies

691 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply

691 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by DF9DQ on Mon Apr 04 02:27:04 MST 2016
The LPC436x was only introduced once silicon revision "A" became available. Revision A is where the CAN errata have been fixed.
This is why there is no mention of these errata for the LPC436x.
0 Kudos
Reply