if is the LPC1765`s SPI not support so high frequece when as slave?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

if is the LPC1765`s SPI not support so high frequece when as slave?

564 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by carson84 on Wed Mar 30 23:23:23 MST 2016
spi port:
p[0].15, --> SCK
p[0].16, --> SSEL
p[0].17, --> MISO
p[0].18, --> MOSI

I use LPC1765`s SPI (slave mode) to communicate with another device.(MTK3360, spi, master mode)
when the clock frequece up to 1Mkz, the LPC1765`s SPI send wrong data out. (below 500KHZ, it is normal)

if is the LPC1765`s SPI not support so high frequece when as slave?
标签 (1)
0 项奖励
回复
1 回复

548 次查看
lpcware
NXP Employee
NXP Employee
bump
0 项奖励
回复