LPC4357 write file to Flash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC4357 write file to Flash

1,642 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by marcosbontempo on Tue May 03 07:17:09 MST 2016
Hello,

I need to develop an application that reads a file in a SD card and write its content to LPC4357 Flash memory.

Do I need to format the LPC4357 memory in some filesystem like FAT?

Is there and example that does it?

Any tip will be very helpful,
Thanks.
标签 (1)
0 项奖励
回复
3 回复数

1,567 次查看
lpcware
NXP Employee
NXP Employee
bump
0 项奖励
回复

1,567 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by marcosbontempo on Wed May 04 04:39:58 MST 2016

Quote: vtw.433e
Use IAP calls (as documented in the User Manual) to write to Flash.

Internal Flash is just linear memory. Only code running on the LPC4357 can access the Flash, so you do not need to format it. You just need to place it into a known location so you can retreive the file and its contents.



Thanks for your answer!

I need to create a file with a path like C://file.txt. Can I do it without a filesystem?

And if I want to write in a external flash, is there an example for it?
0 项奖励
回复

1,567 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vtw.433e on Tue May 03 07:58:58 MST 2016
Use IAP calls (as documented in the User Manual) to write to Flash.

Internal Flash is just linear memory. Only code running on the LPC4357 can access the Flash, so you do not need to format it. You just need to place it into a known location so you can retreive the file and its contents.
0 项奖励
回复