LPC4357 I2S 4-wire issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4357 I2S 4-wire issue

970件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pgeloso on Wed Dec 30 10:29:44 MST 2015

Hi,
I'm having problems with a I2S 4-wire setup using LPC4357 (and LPCXpresso 7.8.0).

I2S0 RX is master and it is sourced by BASE_AUDIO_CLOCK (@12.288MHz to works in stereo mode at 48KHz with 32bit data)
I220 TX is in 4-wire mode.

I correctly see data at the codec output: the transmitter and the codec are running well,  but I always read 0 data in the receiver!
Is there's something wrong in this I2s0 set up?

Could you please double check the register set up?

Thanks
Pietro
//Chip_I2S_RxConfig//Base audio clock and Master. Fig 160 User Manual Rev 2.1
temp=LPC_CREG->CREG6;
LPC_CREG->CREG6 |= (1<<13);//CREG6[13]=1; RX sourcing base_audio_clock

temp = LPC_I2S0->DAI & (~(I2S_DAI_WORDWIDTH_MASK | I2S_DAI_MONO | I2S_DAI_SLAVE | I2S_DAI_WS_HALFPERIOD_MASK));
temp |= I2S_WORDWIDTH_32;
temp |= I2S_STEREO;
temp |= I2S_MASTER_MODE;
temp |= I2S_DAI_WS_HALFPERIOD(31);//bits-1
LPC_I2S0->DAI = temp;
LPC_I2S0->RXMODE = I2S_RXMODE_CLKSEL(1);//01=BASE AUDIO CLOCK
LPC_I2S0->RXBITRATE = 3;
//LPC_I2S0->RXRATE = yDiv | (xDiv << 8);

//Chip_I2S_TxConfig // 4-wire SLAVE of RX.  Fig 152 User Manual Rev 2.1
temp = LPC_I2S0->DAO & (~(I2S_DAO_WORDWIDTH_MASK | I2S_DAO_MONO | I2S_DAO_SLAVE | I2S_DAO_WS_HALFPERIOD_MASK));
temp |= I2S_WORDWIDTH_32;
temp |=  I2S_STEREO;
temp |= I2S_SLAVE_MODE;//I2S_MASTER_MODE;
temp |= I2S_DAO_WS_HALFPERIOD(31);
LPC_I2S0->DAO = temp;
//LPC_I2S0->TXMODE = I2S_TXMODE_CLKSEL(0);//0x0 = Tx fractional rate divider. Select the TX fractional rate divider clock output as the source
LPC_I2S0->TXMODE |= I2S_RXMODE_4PIN_ENABLE;
LPC_I2S0->TXBITRATE = 3;
//pI2S->TXRATE = yDiv | (xDiv << 8);
ラベル(1)
0 件の賞賛
返信
0 返答(返信)