LPC4357 FreeRTOS cause fault after SoftReset

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4357 FreeRTOS cause fault after SoftReset

ソリューションへジャンプ
1,854件の閲覧回数
alessioschisano
Contributor III

Hi, 

I have a little problem on a LPC4357 running FreeRTOS 8.2.

Problem is that when I execute a SoftReset MCU restart but during EMC SDRAM initialization it stop working, with loss of LPC-Link 2 debugger control. So, no HardFault, olny stop ecxecution.

The function where CPU stop working is this: SystemInit_ExtMemCtl (void)

xnxp.JPG

From some research I think it should be a Stack Pointer problem, but not sure about that, FreeRTOS Heap in my application is located in External SDRAM, and if I call the SoftReset routine before FreeRTOS start no problem with EMC init.

xnxp2.JPG

If I made a SoftReset after these instruction, system stop working during initialization in the Reset ISR. 

The same code work right with a LPC4088 in the same condition (Ext RAM FreeRTOS Heap, same reset routine) with no problem.

In LPC 4357 I'm working only with Core M4

Thanks in advance to anyone who could help me.

0 件の賞賛
返信
1 解決策
1,758件の閲覧回数
alessioschisano
Contributor III

Fixed it! Below the solution, hope it helps others in future. Simply need to relocate the MSP and PSP register before resetting:

void (*user_code_entry)(void);
unsigned *p;

void SoftReset(void){

   __disable_irq();

   SysTick->CTRL = 0; // Disable System timer

   // disable and clear pending IRQs
   for (uint32_t i = 0; i < 8; i++)
   {
      NVIC->ICER[i] = 0xFFFFFFFF; // disable IRQ
      NVIC->ICPR[i] = 0xFFFFFFFF; // clear pending IRQ
   }

   // Barriers
   __DSB(); // data synchronization barrier
   __ISB(); // instruction synchronization barrier

   SCB->VTOR = 0x1A010000 & 0x1FFFFF80;

   // Rebase the Stack Pointer
   __set_MSP(*(uint32_t *) (0x1A010000 & 0x1FFFFF80));
   __set_PSP(*(uint32_t *) (0x1A010000 & 0x1FFFFF80));

   p = (unsigned *)(0x1A010000 + 4);
   user_code_entry = (void *) *p;


   __DSB();
   __ISB();

   user_code_entry();
}

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,759件の閲覧回数
alessioschisano
Contributor III

Fixed it! Below the solution, hope it helps others in future. Simply need to relocate the MSP and PSP register before resetting:

void (*user_code_entry)(void);
unsigned *p;

void SoftReset(void){

   __disable_irq();

   SysTick->CTRL = 0; // Disable System timer

   // disable and clear pending IRQs
   for (uint32_t i = 0; i < 8; i++)
   {
      NVIC->ICER[i] = 0xFFFFFFFF; // disable IRQ
      NVIC->ICPR[i] = 0xFFFFFFFF; // clear pending IRQ
   }

   // Barriers
   __DSB(); // data synchronization barrier
   __ISB(); // instruction synchronization barrier

   SCB->VTOR = 0x1A010000 & 0x1FFFFF80;

   // Rebase the Stack Pointer
   __set_MSP(*(uint32_t *) (0x1A010000 & 0x1FFFFF80));
   __set_PSP(*(uint32_t *) (0x1A010000 & 0x1FFFFF80));

   p = (unsigned *)(0x1A010000 + 4);
   user_code_entry = (void *) *p;


   __DSB();
   __ISB();

   user_code_entry();
}

0 件の賞賛
返信