LPC4357 FreeRTOS cause fault after SoftReset

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC4357 FreeRTOS cause fault after SoftReset

跳至解决方案
1,857 次查看
alessioschisano
Contributor III

Hi, 

I have a little problem on a LPC4357 running FreeRTOS 8.2.

Problem is that when I execute a SoftReset MCU restart but during EMC SDRAM initialization it stop working, with loss of LPC-Link 2 debugger control. So, no HardFault, olny stop ecxecution.

The function where CPU stop working is this: SystemInit_ExtMemCtl (void)

xnxp.JPG

From some research I think it should be a Stack Pointer problem, but not sure about that, FreeRTOS Heap in my application is located in External SDRAM, and if I call the SoftReset routine before FreeRTOS start no problem with EMC init.

xnxp2.JPG

If I made a SoftReset after these instruction, system stop working during initialization in the Reset ISR. 

The same code work right with a LPC4088 in the same condition (Ext RAM FreeRTOS Heap, same reset routine) with no problem.

In LPC 4357 I'm working only with Core M4

Thanks in advance to anyone who could help me.

0 项奖励
回复
1 解答
1,761 次查看
alessioschisano
Contributor III

Fixed it! Below the solution, hope it helps others in future. Simply need to relocate the MSP and PSP register before resetting:

void (*user_code_entry)(void);
unsigned *p;

void SoftReset(void){

   __disable_irq();

   SysTick->CTRL = 0; // Disable System timer

   // disable and clear pending IRQs
   for (uint32_t i = 0; i < 8; i++)
   {
      NVIC->ICER[i] = 0xFFFFFFFF; // disable IRQ
      NVIC->ICPR[i] = 0xFFFFFFFF; // clear pending IRQ
   }

   // Barriers
   __DSB(); // data synchronization barrier
   __ISB(); // instruction synchronization barrier

   SCB->VTOR = 0x1A010000 & 0x1FFFFF80;

   // Rebase the Stack Pointer
   __set_MSP(*(uint32_t *) (0x1A010000 & 0x1FFFFF80));
   __set_PSP(*(uint32_t *) (0x1A010000 & 0x1FFFFF80));

   p = (unsigned *)(0x1A010000 + 4);
   user_code_entry = (void *) *p;


   __DSB();
   __ISB();

   user_code_entry();
}

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,762 次查看
alessioschisano
Contributor III

Fixed it! Below the solution, hope it helps others in future. Simply need to relocate the MSP and PSP register before resetting:

void (*user_code_entry)(void);
unsigned *p;

void SoftReset(void){

   __disable_irq();

   SysTick->CTRL = 0; // Disable System timer

   // disable and clear pending IRQs
   for (uint32_t i = 0; i < 8; i++)
   {
      NVIC->ICER[i] = 0xFFFFFFFF; // disable IRQ
      NVIC->ICPR[i] = 0xFFFFFFFF; // clear pending IRQ
   }

   // Barriers
   __DSB(); // data synchronization barrier
   __ISB(); // instruction synchronization barrier

   SCB->VTOR = 0x1A010000 & 0x1FFFFF80;

   // Rebase the Stack Pointer
   __set_MSP(*(uint32_t *) (0x1A010000 & 0x1FFFFF80));
   __set_PSP(*(uint32_t *) (0x1A010000 & 0x1FFFFF80));

   p = (unsigned *)(0x1A010000 + 4);
   user_code_entry = (void *) *p;


   __DSB();
   __ISB();

   user_code_entry();
}

0 项奖励
回复