LPC4357-EVB with LPC-Link2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC4357-EVB with LPC-Link2

3,786 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by biggerfoot on Thu Sep 05 14:19:47 MST 2013
Hi,

I am thinking of buying LPC4357-EVB and LPC-Link2 to start my project. Will they work nicely together with LPCXpresso IDE?

Thanks
标签 (1)
0 项奖励
回复
9 回复数

3,682 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by biggerfoot on Fri Sep 20 16:24:40 MST 2013
Cool. I am gonna buy LPC4357-EVB and LPC-Link2 and have some fun.
0 项奖励
回复

3,682 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Sep 20 15:12:37 MST 2013
I presume that you are asking if LPCXpresso 6 supports the use of LPC-Link2 to connect LPC18/43 targets - the answer to this is yes.

Regards,
LPCXpresso Support
0 项奖励
回复

3,682 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by biggerfoot on Fri Sep 20 10:03:25 MST 2013
LPCXpresso 6 is out, does it include LPC18/43 support?
0 项奖励
回复

3,682 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by whitecoe on Sun Sep 15 06:42:32 MST 2013
It is supported. I am happily using an LPC-Link2 with LPCXpresso IDE here. But the LPC-Link2 functionality in LPCXpresso just doesn't support LPC18/43 as a target MCU yet. - as stated in the FAQ that LPCXpresso Support pointed you at.

HTH!
0 项奖励
回复

3,682 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mhelin on Sat Sep 14 13:09:44 MST 2013

Quote: lpcxpresso-support
Not in the current LPCXpresso 5 release no. As per the other threads previously referenced and the below FAQ, LPC43 will be supported via LPC-Link2 in a forthcoming release.

http://support.code-red-tech.com/CodeRedWiki/LPCLink2support

Regards,
LPCXpresso Support



Hi,

This page says Redlink already is supported by LPCXpresso 5:

http://www.code-red-tech.com/RedSuite5/lpcxpresso-5.php

"JTAG/SWD interfaces supported
Red Probe+,
RDB-Link,
[u]Redlink,[/u]
LPC-Link"

Maybe that is just a typo?
0 项奖励
回复

3,682 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Sat Sep 14 06:18:59 MST 2013
Not in the current LPCXpresso 5 release no. As per the other threads previously referenced and the below FAQ, LPC43 will be supported via LPC-Link2 in a forthcoming release.

http://support.code-red-tech.com/CodeRedWiki/LPCLink2support

Regards,
LPCXpresso Support
0 项奖励
回复

3,682 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mhelin on Sat Sep 14 03:56:33 MST 2013
Hi,

Isn't it possible /supported) if you use Code Red Redlink firmware on LPC Link2?

This link mentions the firmwares:
http://www.embeddedartists.com/products/lpcxpresso/lpclink2.php
0 项奖励
回复

3,682 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Sep 06 00:58:09 MST 2013
Just to expand on this response, the LPC4357 is already fully supported in the current LPCXpresso 5.2.6, but only using the original LPC-Link (or Red Probe+), not via LPC-Link2. There have been a number of threads about this recently ,if you browse or search the forum.

More generally information on LPC43 support can also be found at:

http://support.code-red-tech.com/CodeRedWiki/LPC1850_4350_Support

Regards,
LPCXpresso Support.
0 项奖励
回复

3,682 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Sep 05 21:06:00 MST 2013
A new version of the LPCXpresso IDE, to be released very very soon, fully supports LPC4357.
0 项奖励
回复