LPC4350 SSEL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4350 SSEL

2,270件の閲覧回数
dudisasson
Contributor I

Hi,

I am using an LPC4350 as an SPI slave, is there a way to disable the use of the SSEL pin or drive it to throw another GPIO?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,094件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Please check the below thread and let me know if this helps,

https://community.nxp.com/thread/433611 


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,094件の閲覧回数
dudisasson
Contributor I

Hi,

Thank you for the fast reply.

In the thread you suggested, the LPC is the master so the SSEL is an output

to the slave but In my case the LPC is the slave.

Dudi.

בתאריך 4 בינו׳ 2018 18:15,‏ "soledad" <[email protected]> כתב:

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: LPC4350 SSEL

reply from soledad

<https://community.nxp.com/people/soledad?et=watches.email.thread> in

LPC - View the full discussion

<https://community.nxp.com/message/974577?commentID=974577&et=watches.email.thread#comment-974577>

0 件の賞賛
返信