LPC4350 SSEL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4350 SSEL

2,270 Views
dudisasson
Contributor I

Hi,

I am using an LPC4350 as an SPI slave, is there a way to disable the use of the SSEL pin or drive it to throw another GPIO?

Labels (1)
0 Kudos
Reply
2 Replies

2,094 Views
soledad
NXP Employee
NXP Employee

Hi,

Please check the below thread and let me know if this helps,

https://community.nxp.com/thread/433611 


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,094 Views
dudisasson
Contributor I

Hi,

Thank you for the fast reply.

In the thread you suggested, the LPC is the master so the SSEL is an output

to the slave but In my case the LPC is the slave.

Dudi.

בתאריך 4 בינו׳ 2018 18:15,‏ "soledad" <[email protected]> כתב:

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: LPC4350 SSEL

reply from soledad

<https://community.nxp.com/people/soledad?et=watches.email.thread> in

LPC - View the full discussion

<https://community.nxp.com/message/974577?commentID=974577&et=watches.email.thread#comment-974577>

0 Kudos
Reply