LPC4337 reset error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4337 reset error

3,407件の閲覧回数
luiswalther-aco
Contributor I

Hello, i am Using a LPC4337 with ethernet but i have a problem after reset, when i made a POR (power on Reset) the Microcontrolller works as expected, and the ethernet works fine, but when i made a reset from reset pin or a software reset from the core_reset register than the controller cannot initialize the ethernet, i think that maybe is a bug because i am using a 25MHz external crystal ? because on the LPCxpresso board the Reset from pin dont have any issue.

Thanks

0 件の賞賛
返信
2 返答(返信)

3,110件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Luis Walther-Acosta,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
1. Firstly, I'd like to recommend you check the crystal oscillator circuit by referring to the 13.2 Crystal oscillator section in the attachment.
2. Next, whether you describe the issue in details, as I'm still not very clear with it.
I'm looking forward to your reply.

Ping

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,110件の閲覧回数
luiswalther-aco
Contributor I

Hi jeremyzhou

Thanks for the answer, is solved, I verified  the problem and I was  not initializing my Ethernet PHY correctly, the clock on the LPC4337 are correct, also it was not a problem of the Microcontroller........

0 件の賞賛
返信