LPC4333 JET256 temperature is high when using

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4333 JET256 temperature is high when using

3,514件の閲覧回数
maggiepan
Contributor I

please help solve the problem of LPC4333 JET 256 high temperature in operation, thanks

ラベル(1)
0 件の賞賛
返信
7 返答(返信)

3,352件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Could you please provide more information about your issue.

Which peripherals are you using?

What are you connecting to the MCU?

Are you using a NXP board? If this is no, could you please provide a schematic file?

Please measure the impedance between VDD and Vss.

Please make a visual inspection looking for solder short or open pins.

Please measure the current on the MCU.

Which is the MCU frequency?

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,352件の閲覧回数
maggiepan
Contributor I

Hello, 

Please see below application:

  1. now all the external equipments have been removed when testing;
  2. SDRAM, FRAM, SP706;
  3. please download Schematic from below link: http://pan.baidu.com/s/1kVFUaft ;
  4. VDD 3.28V;
  5. Current 55mA;
  6. No problem has been founded after checking;
  7. Cortext-M4 204MHz; Cortext-M0 204MHz;

Please provide temperature datasheet about this chipset during operation, so that we are able to judge whether the current temperature is normal or not, thanks.

Maggie pan

www.sun-glow.com

[email protected]

0 件の賞賛
返信

3,352件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Maggie

Unfortunately, we doesn't have the chip core frequency with temperature  coefficient data.

We just provide the power consumption with core frequency and temperature related curve:

pastedImage_1.png

Could you provide more detailed data about the chip temperature?

The ambient  temp and the chip surface temp. How about the chip temperature rising ramp?

Thank you.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,352件の閲覧回数
maggiepan
Contributor I

Hello Sir,

Can you provide the register address of [FLASHTIM] bits value of Flash Accelerator Configuration for flash bank A/B? How to operate with it? We couldnt find it as there are lots of register addresses for this chipset.

By the way, can you provide telephone contact info and engineer door-to-door service? it would be quick to solve the problem, thanks.

Best regards,

Maggie pan

www.sun-glow.com

[email protected]

0 件の賞賛
返信

3,352件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Maggie,

Flash Accelerator Configuration for flash bank A register (FLASHCFGA, address 0x4004 3120);

Flash Accelerator Configuration for flash bank B register (FLASHCFGB, address 0x4004 3124).

Following reset, flash accelerator functions are enabled and flash access timing is set to a default value of 16 clocks.

If customer want to modify the [FLASHTIM] value of FLASHCFGA/B register, please refer below code:

LPC_CREG->FLASHCFGA = (0xF << 12) | (0x1 << 31);

LPC_CREG->FLASHCFGB = (0xF << 12) | (0x1 << 31);


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,352件の閲覧回数
maggiepan
Contributor I

Hello Mr. Ma hui,

thanks for your reply.

We tested and found it goes normal when the frequency is lowered to 120Mhz, thanks.

Maggie pan

www.sun-glow.com

[email protected]

0 件の賞賛
返信

3,352件の閲覧回数
maggiepan
Contributor I

it's very urgent

0 件の賞賛
返信