LPC4078 Program Run in BootRom Area,could not jump to "main()"

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC4078 Program Run in BootRom Area,could not jump to "main()"

877 次查看
tangjianbo_cumt
Contributor I

无标题.png

1.png

When under debug mode , use Keil v5,program is always run in "0x1FFF01S2  4201  TST    ri,r0"  ,and this is BootRom . My program could not jump to Main().

The CPU is continue resting ??

标签 (2)
0 项奖励
回复
1 回复

731 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Before answering your question, I'd like to learn more information about this 'issue'. Whether you can clarify these below inquires.
1) Sharing the Option for Target in Keil.
2) Which board and demo you.
3) The voltage status of the ISP pin.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复