LPC3250

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC3250

2,186 Views
K_S_Lin
NXP Employee
NXP Employee

Hi supporters,

      we have a customer who is designing LPC3250 with samsung NAND flash whose part number is K9F4G08F

but failed to access it, I read its datasheet, K9F4G08F is a SLC 4Gbit NAND flash but LPC3250 datasheet says it only support MLC NAND flash with up to 2Gbit flash size. 

pastedImage_1.png

my question is can LPC3250 support this SLC 4Gbit NAND flash?

0 Kudos
Reply
2 Replies

1,889 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello K.S.,

Yes the LPC3250  supports  both  MLC and SLC Nand Flash,   even the board LPC3250 Developer's Kit , contains an SLC Nand flash memory, here is a link:
LPC3250 Developer's Kit | Embedded Artists AB 


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,889 Views
K_S_Lin
NXP Employee
NXP Employee

thanks James

     the ref.design of EA, it uses K9F1G08U0A-P which is a 1Gbit NAND flash, not 4Gbit flash.

would you please to suggest a 4Gbit NAND flash to me? thanks in advance.

0 Kudos
Reply