hello, i have two LPC2364 placed on a board, i want to connect them via ethernet directly withou using of two physical chip. this is possible and what is solution?thanks in advance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

hello, i have two LPC2364 placed on a board, i want to connect them via ethernet directly withou using of two physical chip. this is possible and what is solution?thanks in advance

1,059 Views
johnadams
Contributor I

hello, i have two LPC2364 placed on a board,

i want to connect them via Ethernet directly without using of two physical chip.

is it possible? and what is solution?

thanks in advance.

0 Kudos
Reply
1 Reply

826 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi,

You could directly connect both Ethernet devices without a PHY, connecting TX to RX lines and RX to TX lines. For additional details, you could refer to the following Community link:

https://community.nxp.com/thread/316374

Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply