LPC313xImgCreator.exe utility

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC313xImgCreator.exe utility

1,551 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mnaamat on Thu Jun 27 07:58:07 MST 2013

I need to use the LPC313xImgCreator.exe utility to create image to burn on LPC3141 board via DFU.


Ware can I download this tool?


Miki

标签 (1)
0 项奖励
回复
1 回复

1,445 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kenh6942 on Thu Jun 27 10:26:55 MST 2013

Download the latest LPC313x CDL from this site or lpclinux.com. In lpc3xxx_cdl\csps\lpc313x\tools\ you'll find UnsImgCr.exe. This is to create an unsecure (no AES encryption) image whether booting via DFU or otherwise. I didn't need an encrypted image, so I don't recall what you need to make an encrypted image.


Also keep in mind that the LPC3141 is discontinued as per NXP's website. If you need AES decryption, you should go with LPC3143. Otherwise, go with LPC3130 or LPC3131.

0 项奖励
回复