LPC2468 SD/MMC card interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC2468 SD/MMC card interface

1,431件の閲覧回数
TEMCEFF
Contributor IV

Hello,

Do anyone have standard driver for SD/MMC card interface in LPC2468 micro controller?

If yes please provide the link.

Regards,

Muralidhar

1 返信

1,366件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Muralidhar,

You can download code bundle from the link, but I have checked, it appears that there is not sd card example code.

BR

XiangJun Rong

Single-chip 16-bit/32-bit micro; 512 kB flash, Ethernet, CAN, ISP/IAP, USB 2.0 device/host/OTG, exte...