SCT Timer - selection of fastest processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SCT Timer - selection of fastest processor

Jump to solution
2,629 Views
larsen
Contributor III

I have an application which will benefit from the SCT timer. I would like to have the fastest clock speed available.

Can someone suggest me a processor giving the fastest SCT timer clock speed?

I know the LPC4367 which can operate up to 204MHz.

Are there any faster available now?

Thanks for any hints.

PS: The SCT is a fantastic peripheral for fast timing.

Labels (2)
Tags (1)
0 Kudos
Reply
1 Solution
2,541 Views
jeremyzhou
NXP Employee
NXP Employee

Hi henning larsen ,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
1) Can someone suggest me a processor giving the fastest SCT timer clock speed?
-- The LPC43xx series can't run at overs 204 MHz, and only LPC54628 can run at the 220 MHz now and you can learn more information about it via the below link.
https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mc...

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,542 Views
jeremyzhou
NXP Employee
NXP Employee

Hi henning larsen ,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
1) Can someone suggest me a processor giving the fastest SCT timer clock speed?
-- The LPC43xx series can't run at overs 204 MHz, and only LPC54628 can run at the 220 MHz now and you can learn more information about it via the below link.
https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mc...

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
2,541 Views
larsen
Contributor III

thank you jeremyzhou for your precise and swift answer. Br henning

0 Kudos
Reply