LPC2460 XTAL2 output

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC2460 XTAL2 output

1,144 Views
kevinbooh
Contributor I

We are using the LPC2460 in Slave mode operation with a 12mhz crystal clock oscillator driving the XTAL1 input. In this mode, what is the output of the XTAL2 pin ?

0 Kudos
Reply
1 Reply

1,129 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

For LPC2460, in slave mode, you connect a clock source to the XTAL1 pin via a capacitor Ci with XTAL2 pin float as the following fig:

xiangjun_rong_0-1692165954087.png

In the case, the XTAL2 pin will output a sine signal with the same clock source frequency, but there is a phase-shift.

Hope it can help you

BR

XiangJun Rong

 

 

0 Kudos
Reply