LPC2387

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC2387

1,123 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sumit.kajave on Wed Jul 29 05:11:24 MST 2015
I developed LPC2387 board by own for my home automation project. I burn my IC using flashmagic. In my code I select ROM at address @0x2000 location. My software run on internal oscillator. I developed my code by help of sample code bundle for LPC2300.  My PLL section as below

#define PLL_MValue35
#define PLL_NValue0
#define CCLKDivValue23

/* System configuration: Fosc, Fcclk, Fcco, Fpclk must be defined */
/* PLL input Crystal frequence range 4KHz~20MHz. */
#define Fosc4000000
/* System frequence,should be less than 72MHz. */
#define Fcclk12000000
#define Fcco288000000   

I am using keil uvision5 IDE for my development. 
In simulation my code running properly. But on my board my code doesn't work. I simply toggle port 0. I attach my code below.

Original Attachment has been moved to: lpc_lcd.rar

标签 (1)
0 项奖励
回复
0 回复数