LPC2378 UART0 Rx FIFO Trigger Level problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC2378 UART0 Rx FIFO Trigger Level problem

1,552 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Karthik Venkatesh on Tue Jun 14 16:50:18 MST 2016
Hi,

I am trying to understand the UART0 Receive Trigger level feature available in LPC2378.

Problem Description:

I set FCR register for the Trigger level of 4 bytes.

And reading the IIR register for identifying whether Threshold level interrupt has occured.

If yes, then am reading the RXRBR receive buffer 4 times.

When I run this on LPC2378, for the very 1st byte input, interrupt is triggered.

Find the captured output attached herewith.

What am I doing wrong.

Note: I referred an old thread in this forum reg. the same issue, but in vein.

Code is as following:


#define CR_INTEGER_PRINTF
#include "UART.h"
#include "PLL_CONFIG.h"
#include "PRINT.h"

char a[4];

void UART0_INIT(int baud_rate)
{
        unsigned int k;

        k = SET(baud_rate);

        PCONP |= 1<<3; //power to UART0
        PCLKSEL0 |= 0x40; //pclk = cclk
        PINSEL0 |=  0x00000050;

        U0IER |= (1<<1) | (1<<0);          //Enabling the TX and RX interrupts


        U0LCR = 0x83;

        U0DLM = (k/256);
        U0DLL = (k%256);

        U0LCR = 0x03;

        U0FCR |= (1<<6) | (1<<0);         //Setting the RX Trigger level to 4

}

void send_data(char a)
{

         while(!((U0LSR)&0x20));
         U0THR = a;
}

void get_data()
{

        while(U0IIR & 0x04) {                             //Checking if 'Trigger level reached' interrupt flag is set
              a[0]=U0RBR;                                    //Reading 1st RX Byte from U0RBR
              a[1]=U0RBR;                                    //Reading 2nd RX Byte from U0RBR
              a[2]=U0RBR;                                    //Reading 3rd RX Byte from U0RBR
              a[3]=U0RBR;                                    //Reading 4th RX Byte from U0RBR
              for(char i=0;i<4;i++) {
printf("\n\rChars u entered are %c",a);
              }
        }

}

int main(void)
{

PLL_Config(6,1,12);
UART0_INIT(9600);


while(1)
{

get_data();

delay(300);

}
}


void delay(int delay)
{
int g,k;
for(g=0;g<delay;g++)
for(k=0;k<delay;k++);
}
Labels (1)
0 Kudos
Reply
1 Reply

1,312 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply