LPC2366 versus LPC2368

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC2366 versus LPC2368

ソリューションへジャンプ
2,767件の閲覧回数
bkastelic78
Contributor I

Hi.

Besides LPC2368 having 512kB flash and an SD/MMC support are there any other differences one must take care of? Would like to move from LPC2366 to LPC2368 without any bigger issues.

Thanks

ラベル(1)
1 解決策
2,640件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Yes, right. For details, see :

pastedImage_52.png


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

3 返答(返信)
2,640件の閲覧回数
bkastelic78
Contributor I

Thank you all for your replies. All clear now.

0 件の賞賛
返信
2,641件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Yes, right. For details, see :

pastedImage_52.png


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

2,640件の閲覧回数
bernhardfink
NXP Employee
NXP Employee

With the LPC2368 you will get more flash, an SD-card interface and a USB port.

On top of this it's exactly the same architecture.

Regards,

Bernhard