LPC2214 Replacement Chip

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC2214 Replacement Chip

2,672件の閲覧回数
panneerrajangun
Contributor I

Hi,

As per datasheet, LPC2214FBD144 chip not recommended for new design, For utilizing stock existing PCB we require alternate part number with pin to pin compatible.

Please suggest equivalent part number for the same.

Thank You

Rajan

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,447件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Rajan,

I’m afraid that there are no pin-to-pin replacements for LPC2214FBD144.

However, if you refer to the Product Longevity webpage at the link below, you could check that LPC2214FBD144 part was released on August 2007 and it is a 15-yar longevity device, so, it should be available until 2022:

https://www.nxp.com/products/product-information/product-longevity:PRDCT_LONGEVITY_HM

As other option you could consider reviewing application notes AN10576 “Migrating to the LPC2300/2400 family” and AN10878 “Migrating to the LPC1700 series”.

 

Hope this will be useful for you.

Best regards!

/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,447件の閲覧回数
panneerrajangun
Contributor I

Hi Carlos,

Thank you for your support,

Can we use LPC2292FBD144/01 chip instead of LPC2214FBD144/01?

As per datasheet both chip pin to pin is compatible, LPC2292 have additional CAN feature.

Please suggest the same

Thanks & Regards,

Rajan

0 件の賞賛
返信

2,447件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Rajan,

In such case, yes, they should be compatible, just considering the module differences. You could also refer to User Manual UM10114 for device-to-device comparative of LPC21xx and LPC22xx at the following link:

https://www.nxp.com/docs/en/user-guide/UM10114.pdf


Hope this will be useful for you.

Best regards!

/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信