LPC2214 Replacement Chip

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC2214 Replacement Chip

2,698 Views
panneerrajangun
Contributor I

Hi,

As per datasheet, LPC2214FBD144 chip not recommended for new design, For utilizing stock existing PCB we require alternate part number with pin to pin compatible.

Please suggest equivalent part number for the same.

Thank You

Rajan

Labels (1)
0 Kudos
Reply
3 Replies

2,473 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Rajan,

I’m afraid that there are no pin-to-pin replacements for LPC2214FBD144.

However, if you refer to the Product Longevity webpage at the link below, you could check that LPC2214FBD144 part was released on August 2007 and it is a 15-yar longevity device, so, it should be available until 2022:

https://www.nxp.com/products/product-information/product-longevity:PRDCT_LONGEVITY_HM

As other option you could consider reviewing application notes AN10576 “Migrating to the LPC2300/2400 family” and AN10878 “Migrating to the LPC1700 series”.

 

Hope this will be useful for you.

Best regards!

/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,473 Views
panneerrajangun
Contributor I

Hi Carlos,

Thank you for your support,

Can we use LPC2292FBD144/01 chip instead of LPC2214FBD144/01?

As per datasheet both chip pin to pin is compatible, LPC2292 have additional CAN feature.

Please suggest the same

Thanks & Regards,

Rajan

0 Kudos
Reply

2,473 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Rajan,

In such case, yes, they should be compatible, just considering the module differences. You could also refer to User Manual UM10114 for device-to-device comparative of LPC21xx and LPC22xx at the following link:

https://www.nxp.com/docs/en/user-guide/UM10114.pdf


Hope this will be useful for you.

Best regards!

/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply