LPC2138/2148 bootloader version differences

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC2138/2148 bootloader version differences

3,187 次查看
sutton
Contributor III

Anyone know of a writeup/errata on the code differences/enhancements added between version 2.12 and 2.13?  I think we had a bad batch of chips where reading from code memory gave intermittent errors on LPC2148 chips version 2.12.  We changed to a LPC2138 since we didn't need the USB and the problem completely went away.  We changed one of the failing LPC2148 chips to a new batch of 2138 chips and the problem went away as well.  Not sure that the bootloader changes would have anything to do with chip read errors, but it would be nice to see what was different.  Could have been just a bad batch.

Sutton

标签 (1)
0 项奖励
回复
3 回复数

3,039 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

The only related information I can find is on UM

pastedImage_1.png

For more information, see 

https://www.nxp.com/docs/en/user-guide/UM10139.pdf 


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

3,039 次查看
sutton
Contributor III

The NXP server is not allowing me to respond to your response when

logging in.

400

Your browser sent a request that this server could not understand.

Sutton Mehaffey

Lookout Portable Security

4105 Royal Dr. #100

Kennesaw, GA 30144

770-514-7999

770-514-1285 (FAX)

www.lookoutportablesecurity.com

[email protected]

0 项奖励
回复

3,039 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Sutton,

I can get your reply here without problem.

Jun Zhang

0 项奖励
回复