Eval board for LPC54606J512BD100

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Eval board for LPC54606J512BD100

跳至解决方案
1,662 次查看
joshua_hong
Contributor III

Hi,

is there any eval board for LPC54606J512BD100?

or eval board with pin to pin compatible which can replace with LPC54606J512BD100?

thanks in advance!

标记 (1)
0 项奖励
回复
1 解答
1,587 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Joshua Hong,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is there an eval board for LPC54606J512BD100?
-- No, there're two eval boards for the LPC546xx series, OM13098 and OM13092.

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,588 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Joshua Hong,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is there an eval board for LPC54606J512BD100?
-- No, there're two eval boards for the LPC546xx series, OM13098 and OM13092.

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------