LPC2138/2148 bootloader version differences

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC2138/2148 bootloader version differences

3,125件の閲覧回数
sutton
Contributor III

Anyone know of a writeup/errata on the code differences/enhancements added between version 2.12 and 2.13?  I think we had a bad batch of chips where reading from code memory gave intermittent errors on LPC2148 chips version 2.12.  We changed to a LPC2138 since we didn't need the USB and the problem completely went away.  We changed one of the failing LPC2148 chips to a new batch of 2138 chips and the problem went away as well.  Not sure that the bootloader changes would have anything to do with chip read errors, but it would be nice to see what was different.  Could have been just a bad batch.

Sutton

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,977件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

The only related information I can find is on UM

pastedImage_1.png

For more information, see 

https://www.nxp.com/docs/en/user-guide/UM10139.pdf 


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

2,977件の閲覧回数
sutton
Contributor III

The NXP server is not allowing me to respond to your response when

logging in.

400

Your browser sent a request that this server could not understand.

Sutton Mehaffey

Lookout Portable Security

4105 Royal Dr. #100

Kennesaw, GA 30144

770-514-7999

770-514-1285 (FAX)

www.lookoutportablesecurity.com

[email protected]

0 件の賞賛
返信

2,977件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Sutton,

I can get your reply here without problem.

Jun Zhang

0 件の賞賛
返信