LPC1857 not booting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1857 not booting

3,007件の閲覧回数
vivekpjohn
Contributor II

Hai i am using LPC1857 in a custom designed card. I have followed the hardware design of MCB2300. My board was working well for months and suddenly it stopped working. Since it was working alright earlier, i didnt doubt the hardware design and hence made 4 more such boards. But now none of the boards are working/booting. In JTAG ( i am using both keil ULINK2 and Segger JLINK with KEIL microvision IDE) the core/cpu is not getting detected now. Also, i am not able to get any clock signals in the XTAL1 & 2 pins to which i have connected the 12MHz crystal. Even i tried giving an external oscillator signal to the GP_CLKIN but still not booting.

Can anyone help me out to solve this issue?

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,802件の閲覧回数
vivekpjohn
Contributor II

Hai,

The microcontroller core got detected when i selected SWD instead of JTAG  in the KEIL IDE. But earlier when i was using the prototype board, i was working in JTAG mode. DOn't know why it is not working in JTAG mode now and only in SWD

0 件の賞賛
返信

2,802件の閲覧回数
bernhardfink
NXP Employee
NXP Employee
  • Use boundary scan to check if the device in general is somehow alive
  • Measure the power consumption of a defect board and compare it with a working board (for example when you hold both boards in reset)
  • Remove the chip, reball it and put it into a socket board
  • Talk to your distributor if a quality return of such a defect device is an option
0 件の賞賛
返信

2,802件の閲覧回数
vivekpjohn
Contributor II

Hai,

Thanks for the reply. 

Can you please tell me how to perform the boundary scan test? Is it possible with the JTAG?

Thank you.

0 件の賞賛
返信

2,802件の閲覧回数
bernhardfink
NXP Employee
NXP Employee

I googled for "jlink boundary scan", these are just the first 3 links which I think could show something useful:

How to do a simple JTAG (boundary) scan? - J-Link/Flasher related - SEGGER Forum 

Debugging using Segger J-Link JTAG - Boundary Devices 

JTAG chain & testing 

0 件の賞賛
返信