LPC1833 Oscillator

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1833 Oscillator

2,381 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by fnp-intellegre on Thu Nov 06 11:47:35 MST 2014
Brand new PCB with a LPC1833JET100 populated onto the board. I have applied 3.3V power to the part but see no sine wave on the 12MHz crystal. 18pF load capacitance is present as called out on the datasheet of the Abracon crystal. Are there any specific settings that need to be written before I can see the crystal oscillate ?
Labels (1)
0 Kudos
Reply
3 Replies

2,354 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Thu Nov 06 16:27:41 MST 2014
Hi ,
In you Debugger setting, can you select port as SWD?
0 Kudos
Reply

2,351 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by fnp-intellegre on Thu Nov 06 12:57:54 MST 2014
Paul,

Unable to get the ULINK2 to connect to the LPC1833 using the TCP2030 cable. Schematic attached. Thanks for your help.

0 Kudos
Reply

2,351 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Paul on Thu Nov 06 12:38:39 MST 2014
The default clock for the LPC18xx is the internal RC oscillator, so you will not see the crystal oscillate until you change the clock source to the external crystal oscillator.  See the Clock Generation Unit (CGU) chapter for details.

Paul
0 Kudos
Reply