LPC1833 Oscillator

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1833 Oscillator

2,441 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by fnp-intellegre on Thu Nov 06 11:47:35 MST 2014
Brand new PCB with a LPC1833JET100 populated onto the board. I have applied 3.3V power to the part but see no sine wave on the 12MHz crystal. 18pF load capacitance is present as called out on the datasheet of the Abracon crystal. Are there any specific settings that need to be written before I can see the crystal oscillate ?
标签 (1)
0 项奖励
回复
3 回复数

2,414 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Thu Nov 06 16:27:41 MST 2014
Hi ,
In you Debugger setting, can you select port as SWD?
0 项奖励
回复

2,411 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by fnp-intellegre on Thu Nov 06 12:57:54 MST 2014
Paul,

Unable to get the ULINK2 to connect to the LPC1833 using the TCP2030 cable. Schematic attached. Thanks for your help.

0 项奖励
回复

2,411 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Paul on Thu Nov 06 12:38:39 MST 2014
The default clock for the LPC18xx is the internal RC oscillator, so you will not see the crystal oscillate until you change the clock source to the external crystal oscillator.  See the Clock Generation Unit (CGU) chapter for details.

Paul
0 项奖励
回复