LPC1833 - How set Drive strength of normal drive pins?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC1833 - How set Drive strength of normal drive pins?

跳至解决方案
677 次查看
ketulpatel
Contributor II

Hello,

We are using LPC1833.

We want to set Pin P6_5 with High-drive strength, but as per user manual this Pin P6_5 is not in the list of Pin configuration registers for high-drive pins.

How we can set it using software or need to set using it hardware?

 

ketulpatel_2-1732864818839.png

Thanks.

0 项奖励
回复
1 解答
658 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello @ketulpatel 

P6_5  is normal drive pin and we can't set it to high drive, the limit is on chip design.

According to UM, The pin configuration registers for high-drive pins control the following pins:
• P1_17
• P2_3 to P2_5

• P8_0 to P8_2
• PA_1 to PA_3

Hope this will help you,

Jun Zhang

在原帖中查看解决方案

0 项奖励
回复
2 回复数
659 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello @ketulpatel 

P6_5  is normal drive pin and we can't set it to high drive, the limit is on chip design.

According to UM, The pin configuration registers for high-drive pins control the following pins:
• P1_17
• P2_3 to P2_5

• P8_0 to P8_2
• PA_1 to PA_3

Hope this will help you,

Jun Zhang

0 项奖励
回复
651 次查看
ketulpatel
Contributor II
Thanks ZhangJennie for the quick response.
0 项奖励
回复