LPC1833 - How set Drive strength of normal drive pins?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1833 - How set Drive strength of normal drive pins?

ソリューションへジャンプ
736件の閲覧回数
ketulpatel
Contributor II

Hello,

We are using LPC1833.

We want to set Pin P6_5 with High-drive strength, but as per user manual this Pin P6_5 is not in the list of Pin configuration registers for high-drive pins.

How we can set it using software or need to set using it hardware?

 

ketulpatel_2-1732864818839.png

Thanks.

0 件の賞賛
返信
1 解決策
717件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello @ketulpatel 

P6_5  is normal drive pin and we can't set it to high drive, the limit is on chip design.

According to UM, The pin configuration registers for high-drive pins control the following pins:
• P1_17
• P2_3 to P2_5

• P8_0 to P8_2
• PA_1 to PA_3

Hope this will help you,

Jun Zhang

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
718件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello @ketulpatel 

P6_5  is normal drive pin and we can't set it to high drive, the limit is on chip design.

According to UM, The pin configuration registers for high-drive pins control the following pins:
• P1_17
• P2_3 to P2_5

• P8_0 to P8_2
• PA_1 to PA_3

Hope this will help you,

Jun Zhang

0 件の賞賛
返信
710件の閲覧回数
ketulpatel
Contributor II
Thanks ZhangJennie for the quick response.
0 件の賞賛
返信